(0)| 4/15/2021 6:25 PM | |
|
Joined: 9/22/2017 Last visit: 10/24/2025 Posts: 8 Rating:
|
Hi, Anyone has idea if it is possible to set a bit or digital tag when a particular alarm is acknowledged
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/16/2021 09:43:55New subject after splitting |
|
| 4/28/2021 10:45 AM | |
|
Posts: 7298 Rating:
|
Hello Anirudh7Nov, you can configure an "acknowledgment tag/bit" for every single message. The message was acknowledged if the corresponding acknowledgment bit has the value "1". see the manual "SIMATIC HMI WinCC V7.5 SP1 WinCC Information System" https://support.industry.siemens.com/cs/ww/en/view/109772961/60524003851
Georg Berghof |
| 4/28/2021 2:42 PM | |
|
Posts: 198 Rating:
|
Hello Anirudh, There are multiple options to perform this and it depends on your requirement whether you would like to create a separate button to acknowledge the alarm and set a bit or tag as a consequence of that. In this case, you have to create a custom button in the desired location (or customized alarm control) and when you click the button to acknowledge, you can set a bit on 'mouse button click' and reset it on the release of the click. However, if you want to set the bit when any alarm from Alarm Logging list was acknowledged by the corresponding button in the toolbar, there is a different way to do it - using Status Tag of a Message Group. Every alarm message occupies two bits in the status tag - The 'ack' bit is one while the other is one activated/deactivated or came in/went out status. The position of the "acknowledgment bit" depends on the data type of the status tag. It is better to use a 32 bit unsigned integer tag for status. If the status tag is of data type "32 bit unsigned" and the status bit = 9, ● bit 9 of the status tag indicates the "Came In / Went Out" state of the message group. ● bit 25 of the status tag indicates whether the message group contains a message requiring acknowledgment that has not yet been acknowledged. This concept of status is well explained in the Working with WinCC Manual under the section 'Configuring the Message System'. Hope this helps |
Last edited by: Jen_Moderator at: 04/29/2021 07:18:49Optimized link. |
|
Follow us on