(0)| 5/2/2021 2:07 PM | |
|
Posts: 2 Rating:
|
hi I have an ES station with windows 7 ultimate and pcs7 8.1 sp1. I have a problem with CPU-rt fb128 .this function must be generated in the entire CFC compile. this is a system function( @cpu-rt).but when I do the entire compile with generating module drive don't generate this function! ( other system functions like @1 @2,... generated). I remove the ES-MAP function and all system functions ( @) and do the entire compile with generating module drive again, but this function doesn't generate! also, I don't have any warning and alarm, and error in CFC entire compile with module drive. also, I have this function in Blocks (FB128) and I do block type function in CFC. also, check another Same project .that is fine and everything ok. but don't solve this problem. how can I generate this function? ------------------------------------------------------------------------------------------ |
Last edited by: nbahman at: 05/02/2021 14:15:02Last edited by: Jen_Moderator at: 05/03/2021 11:34:28New subject after splitting |
|
| 5/4/2021 8:07 AM | |
|
Joined: 3/14/2008 Last visit: 1/15/2026 Posts: 2233 Rating:
|
Hi, Which firmware does your CPU have where CPU_RT must be used? The CPU_RT can only function when the firmware is >=5.0 (for single AS) or >=4.5 (for H controller). You can check if you have SFC 78 in your blocks folder.
|
Last edited by: Oreca at: 05/04/2021 08:08:51If I could help you, you can use the RATE button. Thank you. |
|
Follow us on