(0)| 5/15/2021 5:38 AM | |
|
Joined: 3/28/2015 Last visit: 1/4/2026 Posts: 727 Rating:
|
Hello, Have a look at the following topic: Sales release and download of firmware 3.2 for CP 1242-7V2, CP 1243-7 LTE, CP 1243-1, CP 1243-8 IRC ---------------------------------------------------------------------- 6GK7242-7KX31-0XE0_V03.02.24_OSS.zip(69.7 MB) Procedure for updating the CP firmware: You can either install the firmware update via the STEP 7 online diagnostics functions, or create a SIMATIC memory card from the Siemens customer support website from which you can download the firmware update. This process is described in the S7-1200 system manual. Step7 V16 and higher (TIA Portal) is to be used for configuration of the modules with firmware 3.2. ------------------------------------------------------------------------ |
|
Eng.Mohamed Ibrahim |
|
Follow us on