(0)| 5/18/2021 7:48 PM | |
|
Joined: 3/14/2008 Last visit: 1/15/2026 Posts: 2233 Rating:
|
Hi, You have two options to migrate: software update with or without new functions. If you want to use new functions, follow the manual under this link. I suggest you update also to Update Collection 2 which is the latest update for SP3. You can download it from the site. |
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
|
|
| 5/19/2021 8:10 AM | |
|
Posts: 101 Rating:
|
Sure, Thank you..!! 1. As I am using CMT as I understand, I need to first migrate CMT library 2. Then CMT charts in a project with project compile 3. But I am not clear like how should i migrate OS project. 4. For 2nd point I mention in question, Do you have any suggestion? I am new to migration concept, sorry for too many questions. Can I directly copy CMT chart from PCS7 v9.0 sp1 to PCS7 sp3? Thanks, Zankkar |
Last edited by: Zankkar at: 05/19/2021 11:45:23 |
|
| 5/19/2021 8:23 AM | |
|
Joined: 3/14/2008 Last visit: 1/15/2026 Posts: 2233 Rating:
|
Hi, It is quite a procedure for updating, but roughly: 1. Copy blocks from AP Library new version to master library project 2. Update block types in CFC (All blocks from AP Library are updated with new version (you have to check if a PLC stop is needed) 3. Update CFC charts to newest version (when the project is opened on the new version, open a CFC and move a block one position, then CFC popups a message that you need to migrate to new version) 4. Update blocks from master library to project(s) via Update Block Types. 5. Open OS project and execute OS project editor (so new files like faceplates/block icons are updated in the project). 6. etc. you can find this in the manual. Best thing is to read through the manual since everything is listed there so you won't forget something.
|
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on