(0)| 5/24/2021 4:53 AM | |
|
Joined: 5/9/2015 Last visit: 3/18/2025 Posts: 81 Rating:
|
Hello, Pls check page 31 and 46 in the attached configuration manual. Hope this will be helpful for you. Best regards, nkr Attachmentps7phosb_en-US.pdf (1292 Downloads) |
| 5/25/2021 9:02 AM | |
|
Posts: 198 Rating:
|
Hello, A reference OS makes use of another OS as a basis (base OS). You can configure a reference OS for OS single station systems and OS clients. The configuration procedure for OS Single station or clients differs with the object being added in the PC station configuration. The major configuration involves: ● Inserting and configuring the reference OS ● Assigning the reference OS to the base OS. You can find more information about the use of reference OS in section 4.4 and the configuration procedure in section 6.1.7 in the manual linked below: SIMATIC Process Control System PCS7 Operator Station Manual Hope this helps |
Follow us on