(1)| 6/1/2021 12:28 AM | |
|
Posts: 2 Rating:
|
Hello, I did already checked that post, however, it seems it only works with TIA Portal v13. I tried to import the file to TIA Portal V16, unfortunately it requires a previous upgrade by using TIA Portal v13 SP1/SP2. Has anyone else dealed with it? Is there other possible way to use 4 to 20 mA signal with hardware designed to work with 0 to 20 mA signals? Will appreciate any clue. Thanks in advanced. Best regards, Jose ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/01/2021 09:17:29New subject after splitting |
|
Follow us on