(0)| 2/24/2009 9:19 PM | |
|
Joined: 2/24/2009 Last visit: 11/21/2025 Posts: 41 Rating:
|
greetings ladies want to design a SCADA system but commanded by pc (I have since some bikers from the PC and monitor analogue signals), the truth I have no esque conosimiento in and just made some minor aplicaiones with rsview32 My idea is to place a plc 224xp cpu module connected to an ethernet em243 which would connect to pc via lan. my doubt is that software and if there are any hold on their use titurial att PD: I made the translation with the google tool
I leave here an example http://www.imaxenes.com/imagen/scada1qw88vm.gif.html |
| 2/25/2009 10:45 AM | |
|
Joined: 5/8/2006 Last visit: 10/23/2025 Posts: 1085 Rating:
|
Hi You should know that WinCC flexible is not a SCADA system butWinCC is a SCADA system. So, you can use a S7-224 XP in combination with a CP243-1 an the WinCC flexbile Runtime or WinCC Runtime. If you use only a S7-224 XP CPU in your project I think that WinCC flexible is sufficientin this case. FAQ - Information about the communication betweenS7-200 and WinCC flexible: http://support.automation.siemens.com/WW/view/en/19724696 Information about WinCC flexible project planning: http://support.automation.siemens.com/WW/view/en/18660846 http://support.automation.siemens.com/WW/view/en/18656980 http://support.automation.siemens.com/WW/view/de/18657078 I hope that I could help you. Bye |
Follow us on