6/14/2021 2:22 PM | |
Joined: 7/9/2018 Last visit: 2/16/2025 Posts: 7 Rating:
|
Hello, I have established communication between logo s8 and s7 -1214. S7 is server in my network, just like in this example. My question is how can i control the same variable on both devices. For example i use counter on logo to store value. This value is getted from s7( to be exact from webserver ), so the driection is logo8 <- s7. But i also have to have posibilty to change this value from logo by messege text and update variable in s7. If i leave it as now i have possibility to change value in s7 or if i change direction only form logo. How should i create connection to have posibilty changing value from both devices and sending it in both dricection. Thanks in advanice for any tips. |
6/14/2021 2:34 PM | |
Joined: 7/9/2018 Last visit: 2/16/2025 Posts: 7 Rating:
|
Thanks for making me aware. |
This contribution was helpful to
1 thankful Users |
Follow us on