(0)| 2/20/2009 12:54 PM | |
|
Posts: 4 Rating:
|
Hi I like to make a redundant network with two exsternal units (MRU's - Motion Reference Unit) communicatingon RS232 or RS422 with a redundant S7-400 node. As I can sethere is two alternatives: 1. Tomake the programming part easier,convert the signal to profibus and thenvia Y-link. 2. UseRS422 and make multi drop connection to CP440-1 point-to-point connection cards. Please see attached suggestions. Is there a better way to solve this? AttachmentVisio-MRU.pdf (274 Downloads) |
| 2/25/2009 2:19 PM | |||
|
Posts: 124 Rating:
|
You could use alternative 1, with only one redundant network (you don't need two networks in each CPU) with ET200M and two CP 341 in the ET200M
Regards Mario Braganca www.exco.de |
||
Follow us on