(0)| 6/19/2021 7:02 PM | |
|
Posts: 1 Rating:
|
I have two problems: 1) I cannot get a correct PLC reset When at the end of PLC clearing procedure I switch S4 from 3 to 2-3-2 and after blinking PS I wait when PF lightsUp but no sucess - PF does not light up. 2) I cannot get "6" on the seven-segment display "H3" I try second variant to general reset all PLC and NCK (S3 to 1 S4 to 3, then turn on, wait my "b" and push S1 reset button, wait my "b" on H3 then turn off S3 to 0, 15 sec wait, turn on wait my H3 "b" and make first reset procedure with 2-3-2 by S4) and get H3 "b". I try remove battery and wait one houre or short-circuit the capacitors. any variants do not get me see "6" on H3 I do not try reset from simatic step 7, I do not now how it work I just have nulmodem cabel to connect winpcin to V24 and all. May be from its way I can get much more information about it trouble (can read some diagnose) I get some errors, but I do not now which from it true, becouse, when I reload nck and plc its change. And at the end anybody really now - my NCU must have memmory card yes or now, I ask it because I find it description - https://support.industry.siemens.com/cs/document/4230176/810d-sw-release-2-4-release-for-delivery?dti=0&lc=en-UA and here is PC card, but in my case I do not have it may be it lost I do not now history of it machine. I make some photos videos of it machine https://photos.app.goo.gl/seURYRTh9Y6icv749 and VIDEO https://www.youtube.com/watch?v=iTMWvr5ek0U |
Follow us on