(0)| 6/21/2021 9:48 PM | |
|
Joined: 9/9/2015 Last visit: 12/5/2025 Posts: 732 Rating:
|
Hi spikestar, I never see it before. Can you show us a few pictures on it? any error codes? and installed software as well. May be you can consider a PCS 7 upgrade too. Make sure your system is matching with the compatibility list. |
|
Please give me 5 stars Rating if my post is helpful for you. :) |
|
| 6/21/2021 10:17 PM | |
|
Joined: 3/14/2008 Last visit: 1/15/2026 Posts: 2233 Rating:
|
Hi, I have gotten this error a few times, even with PCS7 V9.0 SP3. It has something to do with the SQL database, where the plant hierarchy does not have connection to the database. Only solution as you explained is to restart the project. Inserting CFC charts is not possible as well. It has nothing to do with compatibility issues because my installation was setup correctly. Sometimes a similar situation can also happen when you have a Vmware and you resume it after pausing (not allowed by the way). But if this happens often, you can create a SR. Also Siemens will ask you to run the Assessment Suite to collect data from your system in order to pinpoint the problem. Sorry, but no real solution. |
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
|
|
Follow us on