(0)| 6/20/2021 8:41 AM | |
|
Posts: 19 Rating:
|
Dear all I am having a problem with servo spindle. When I press Jog key (from MCP) , the spindle start with a jerk, then stop eventually and produced a drive alarm F7900 on servo drive. If I press a reverse spindle command it first try to rotate opposite direction and then it try to rotate commanded direction, for this reason it produced a shock and then stop with alarm F7900 on the drive seven segment display. This whole things happen within a second. Also I am getting alarms on CNC screen are 021612 & 025201. During the drive configuration I have only option for motor ID 20001 but my spindle motor ID is 20004. I have no option for configuring my ID 20004 motor. I have checked my encoder cable, motor shaft for checking it can rotate freely and encoder pulse. But I have not checked the motor torque limit & inversion of the actual value [ Please clarify this two parameter as I am not familiar with this two] I have set the parameter 32260, 32000, 26200, 31050, 31060. Before this new setting the spindle was working fine. Please help me to solve this issue. Please clarify which parameters are important to commissioned servo spindle. Kind Regards ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/21/2021 08:32:00New subject after splitting |
|
Follow us on