(0)| 6/28/2021 9:00 AM |
|
|
Joined: 12/27/2018 Last visit: 10/5/2025 Posts: 510 Rating:
|
https://www.google.com/amp/s/www.indiatoday.in/amp/india/jammu-and-kashmir/story/jammu-drone-attack-air-force-station-ied-probe-update-development-1820181-2021-06-28 Drones dropped 2 kg highly explosive IEDs on Jammu Air Force station | 10 pointsProbe has intensified into the drone attack on Jammu Air Force station. Initial probe has found that drones were used to drop ‘impact’ IEDs at the air base. Use of RDX, which is not available in India and usually sourced from Pakistan, is also being suspected by security agencies investigating the attack at Jammu base.Siemens PLC could be linked in any news future. May be more advanced. Can. You imagine if it happened to siemens HQ |
Last edited by: JKV JAMES ❤️(König James) at: 06/28/2021 09:05:00Last edited by: JKV JAMES ❤️(König James) at: 06/28/2021 09:09:06Jinson James, M.Tech (Power Electronics and Power System), |
|
Follow us on