(0)| 6/24/2021 11:42 AM | |
|
Posts: 1 Rating:
|
Dear All, Kindly suggest me, I have a Analog module 6ES7134-6GF00-0AA1 and Base unit 6ES7193-6BP00-0BA0, Now i don't have any Base Unit with Aux Terminals so how can do four wire wiring?? With above given Base unit, we can do four wire connection or not?? if Yes so kindly post for me How? Because I am doing this with above base unit as per Manual 2 wire connection Like I0+ & Uv+ and aux supply from outside device but my device is not working ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/24/2021 12:29:55New subject after splitting |
|
| 7/5/2021 12:05 PM | |
|
Joined: 3/11/2019 Last visit: 1/7/2026 Posts: 1653 Rating:
|
Hi, as shown in the manual, the AUX terminals are connected to "ground" of the module. So basically it should work if you connect the sensor to the same "ground" which used by the module by using seperate/external clamps for ground. SIMATIC ET 200SP analog input module AI 8xI 2-/4-wire BAregards sancruz |
|
Feedback appreciated, please rate |
|
| 7/5/2021 1:35 PM | |
|
Posts: 5521 Rating:
|
hi, as sancruz suggested, the AUX-terminals are only to deliver the ground-potential. You can take this potential from anywhere else too. regards, |
Follow us on