(0)| 7/5/2021 11:40 AM | |
|
Posts: 2 Rating:
|
Hi! I have problem with sinumerik 828D. I make a tuning programm in ISO mode. the part of program where is only turning operation everything is o.k, last operation is milling. An machine this operation wont do. Error “16410 Channel 1: Block324 axis Y is not a geometru axis”. If this last operation, where is only milling operation, i make like a new program, everything is working. This is milling part: (TOOL - 12 OFFSET - 1) (6 FLAT ENDMILL) G55 G0 T12 G19 C3=0. SETMS(2) G97 S5000 M3 G0 Z35. X217. Y-39. X177. G98 G1 X167. F600. Y39. F300. G0 X217. X217. Y-39. Z35. C3=120. X177. G1 X167. F600. Y39. F300. G0 X217. X217. Y-39. Z35. C3=240. X177. G1 X167. F600. Y39. F300. G0 X217. G0Y0 G28 U0. M05 G28 W0. G291 M30 ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/05/2021 13:37:22New subject after splitting |
|
| 7/9/2021 1:52 PM | |
|
Posts: 2 Rating:
|
I have separate Y axis. After G28 i set TRAANG() and everything is working! |
Follow us on