(0)| 8/4/2021 1:28 PM | |
|
Posts: 3 Rating:
|
Yes I have same problem now. Is there anyone for help us |
| 8/4/2021 8:27 PM | |
|
Joined: 3/14/2008 Last visit: 12/28/2025 Posts: 2233 Rating:
|
Hi, Please attach the compilation log and all diagnose files during the time of the compilation, I can take a look at them. Compilation log can be found under: [Project name of the server]\wincproj\[Name of WinCC application and is called: "TRANSFER.log". You can also access it by selection the WinCC application and right click: Display compilation log. Diagnose files can be found under: C:\Program Files (x86)\SIEMENS\WinCC\diagnose If I cannot find anything related to the error, you can also create a SR. Please open the following link. It's about the Siemens Assessment Suite and it's software (that does not have to be installed) that collects system information and software information. You can upload the logfile that is generated to your SR. |
Last edited by: Jen_Moderator at: 08/05/2021 07:28:26Optimized link. If I could help you, you can use the RATE button. Thank you. |
|
| 8/7/2021 10:11 PM | |
|
Posts: 3 Rating:
|
Hi Oreca I am sending the report prepared by Siemens Assessment Suite AttachmentSAS.txt (128 Downloads) |
| 8/8/2021 10:38 PM | |
|
Joined: 3/14/2008 Last visit: 12/28/2025 Posts: 2233 Rating:
|
Hi, Can you upload the diagnose file from the compilation log and files under "diagnose" folder as I explained in my previous post? The log from the assessment suite can be attached to your SR. But first I would like to see the compilation log and diagnose files. Thanks! |
|
If I could help you, you can use the RATE button. Thank you. |
|
| 8/11/2021 9:41 AM | |
|
Posts: 3 Rating:
|
All logs in diagnose folder are here [snip] Attachmentdiagnose.zip (138 Downloads) |
Last edited by: Jen_Moderator at: 08/11/2021 12:41:19Removed link and added file as an attachment. |
|
| 8/11/2021 3:00 PM | |
|
Joined: 3/14/2008 Last visit: 12/28/2025 Posts: 2233 Rating:
|
Hi, Can you upload the TRANSFER log? I did not see that one. This is the compilation log when you start WinCC compilation. Please upload. Are you using Windows 8 as operating system? I see some information about Windows 8 in the logs. |
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on