(0)| 8/16/2021 4:54 PM | |
|
Posts: 1 Rating:
|
Hello! I am quite new in the community and have a problem regarding the implementation of a Back Button in a Faceplatte with Unified V17. I noticed that the "ChangeScreen" function is not directly available on the Faceplatte, so I created a Bool Tag "BackButton" which changes its value when a button in the Faceplate is pressed. I get the value outside of my Faceplate, then I tried to trigger my ShowPreviousScreen Script through "Scheduled Task" but the UI Object is not recognized and it keeps showing compiling errors. Do you know which other way I can trigger the script when the button in a faceplate is pressed? * The ShowPreviousScreen Script is already working when attached to a Back Button outside of the Faceplatte, but I want to explore its functionality as part of a Faceplate. ------------------------------------------------------------------------------------------ |
Last edited by: AutoGen_2904263 at: 08/16/2021 17:01:43Last edited by: Jen_Moderator at: 08/17/2021 07:17:17New subject after splitting |
|
Follow us on