(0)| 10/9/2021 3:40 AM | |
|
Posts: 6 Rating:
|
Good evening, colleagues. I am facing the same problem with the RED670, REB500 integration in SicamPas 8.14. When I unload a substation scd file from PCM600_2.10 and load it in SicamPas 8.14 I get the following errors Starting the error report for 1.IED...;10/8/2021;4:28:58 PM; The validation of IED 'SEA2TCPMRED1' (device type: 'IED670' from manufacturer: 'ABB') is finished with errors.;10/8/2021;4:28:58 PM; Contact your 'ABB' support to solve the problem.; Error at line 897, char 8 --> '<ReportControl name="rcbStatUrg" desc="PCM600 auto-generated RCB" datSet="StatUrg" confRev="500" intgPd="3000" bufTime="100" buffered="true">';10/8/2021;4:28:58 PM; ('Message: The required attribute 'rptID' is missing.'); Error at line 904, char 8 --> '<ReportControl name="rcbStatNrml" desc="PCM600 auto-generated RCB" datSet="StatNrml" confRev="400" intgPd="3000" bufTime="100" buffered="true">';10/8/2021;4:28:58 PM; ('Message: The required attribute 'rptID' is missing.'); Error at line 911, char 8 --> '<ReportControl name="rcbMeasFlt" desc="PCM600 auto-generated RCB" datSet="MeasFlt" confRev="300" intgPd="3000" bufTime="100">';10/8/2021;4:28:59 PM; ('Message: The required attribute 'rptID' is missing.'); Ending the error report for 1.IED.;10/8/2021;4:28:59 PM; What can you advise to solve this problem? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/11/2021 10:36:10New subject after splitting |
|
| 10/11/2021 10:37 AM | |
|
Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject Problem with the RED670, REB500 integration in SicamPas 8.14 is published within the conference Meet & Talk. Jen_Moderator |
Follow us on