10/19/2021 6:37 AM | |
Joined: 10/14/2014 Last visit: 5/17/2024 Posts: 26 Rating: (0) |
Another question about the simulation ... Maybe it already happened ... When simulating an HMI project using PLC-SIM in trends, integer variables go all the time (300 seconds) from the left edge to the right, and the real ones - only a few tens and seem to stop seconds, but if you change data, then on this visible area they change adequately. What is it? Conducted several experiments on changing data types in trend properties. It turned out that this does not depend on the data type. To exclude possible inattention, I made a copy-paste from the working trend and inserted other integer data into it - the data also became not for the entire length of the chart (300 seconds), but only for 25-30 seconds. I carry out the simulation with the panel type IPC477D, WIN CC Advanced TIA15 I apologize, perhaps the moderator needs to move this post to another topic. ------------------------------------------------------------------------------------------ |
Last edited by: Mr_Frodo at: 10/19/2021 07:06:46Last edited by: Mr_Frodo at: 10/19/2021 07:08:08Last edited by: Mr_Frodo at: 10/19/2021 08:39:31Last edited by: Jen_Moderator at: 10/19/2021 12:13:58New subject after splitting |
|
This contribution was helpful to1 thankful Users |
Follow us on