(0)| 10/12/2021 5:22 PM | |
|
Posts: 6 Rating:
|
Good afternoon, colleagues. We have the task of transferring part of the tags received via the S7 protocol from Sicam SCC to Sicam PAS. We need to solve it as soon as possible. Sicam PAS is licensed only for IEC 61850, IEC 104, Modbus Master and Automation. Please tell me how to transfer the required number of tags from Sicam SCC to Sicam PAS, because these tags need to be transferred further via IEC 104 and also via DNP3.0. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/18/2021 07:12:53New subject after splitting |
|
Follow us on