(0)| 8/15/2013 11:03 AM | |
|
Posts: 3 Rating:
|
Dear Experts and community, during the first compilation of a newly setup OS i get the above error message without any further explanation. In the compilation log the error occurs always with the first Tag he would have to create from the CFC programm. To be certain it has nothing to do with this specific tag i removed that cfc from the programm, recompiled CFC and then again WinCC. Same error just at the now first Tag from CFC. PLC and OS objects are set up communicate through industrial Ethernet using TCP/IP, connection is displayed correctly and can be selected without any trouble. The most disturbing fact is that there is no explanation whatsoever. Is there any place where i can find the error numbers to find out, what could be the actual problem? I also migrated one of my former multiprojects done in 7.1 Sp3 and tried a complete compile including memory reset just to check if the problem might be in the PCS7 installation, or operating system, but that works just fine. So i assume it has to be some issue with the communication path or any detail concerning the protocol suite, but without a translation for the error code ican only guess, since everythings seems to be in order as far as i can see. logfile attached AttachmentLOG.zip (295 Downloads) |
| 11/5/2013 4:49 PM | |
|
Joined: 7/26/2006 Last visit: 9/22/2025 Posts: 7 Rating:
|
Hello Nordwind How do you get out of this Problem? |
| 9/5/2014 5:41 AM | |
|
Joined: 7/19/2013 Last visit: 11/17/2025 Posts: 76 Rating:
|
Hi All, I solved the same problem with entire compilation in AS and OS Regards, Ronaldo7 |
Follow us on