(1)| 12/17/2021 11:24 PM | |
|
Posts: 257 Rating:
|
Hello SIOS Forum Community In the S7-300 CPUs, MC (Memory Card) and MMC (Micro Memory Card) are used as memory cards. Only SIMATIC Micro Memory Cards (MMC) are used in the interface modules (IM) and base modules (BM) of the ET 200 series with CPU functionality. An MC can be used with older S7-300 CPUs with MC slot. The size is approx. 57mm x 45mm x 7mm. An MMC is mandatory for the operation of all current S7-300 CPUs. The size is approx. 32mm x 24mm x 1mm Further information: Which memory cards can you use with an S7-300 CPU? Which memory cards are used with ET 200 interface modules with CPU functionality? Information on how to read a memory card outside of S7-300 CPUs can be found here. Best regards, SIMATIC International Technical Support Hub. |
Last edited by: SIMATIC International Technical Support Hub at: 12/17/2021 23:33:41 |
|
This contribution was helpful to
|
|
Follow us on