(0)| 12/21/2021 11:16 AM | |
|
Joined: 6/12/2017 Last visit: 7/19/2023 Posts: 3 Rating:
|
Hi This is Pambos .It is my first time here.I have a relative question to the above.I want to directly connect an IEC61850 device to SCC. I have created a new suite for IEC as described in the previous question.I imported successfully the scd file of the IED , i have seen all my signals in the TAG management ,I pinged the IP address of my IED successfully but unfortunately my signals are not updated.It is obvious that I need to set somewhere some comm. attributes.Can anybody help? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/21/2021 13:31:29New subject after splitting |
|
Follow us on