(0)| 12/15/2021 6:41 AM | |
|
Posts: 8092 Rating:
|
Hello Griffis714, Is it from Siemens or third party key board? Siemens standard key board is MCP483C (not KB) mechanical type & order number is 6FC5203–AF22–0AA2. Yes, key board device is plug & play type only & keys are internally decoded in PLC logic. So please check if it is from Siemens or by third party. Since you mentioned, machine run normally before replacement of keyboard, I suggest you to check & compare, old & new keyboard article numbers (in case if it is Siemens standard keyboard). If you need help, please post the nameplate snaps of old & new keyboard so that forum member can help you. Hope this helps. |
Last edited by: PISCEAN 2010 at: 12/15/2021 08:31:53Corrected post for keyboard specification type :-( |
|
| 1/5/2022 2:54 PM | |
|
Posts: 4 Rating:
|
UPDATE: We have reordered a new keyboard and installed it. Everything seems to be functioning properly. The issue must have been a faulty repair part. |
Follow us on