(0)| 3/23/2009 11:29 AM | |
|
Joined: 5/8/2006 Last visit: 10/23/2025 Posts: 1085 Rating:
|
Hi if you want to communicate with an ABB plc over Profibus you canuse the SIMATIC S5 DP driver because this driver communicates over the IO address range. The communication via OPC is possible, too. (2) You can use structured tags only with faceplates.You should know that you canuse only internal structures and in connection with the SIMATIC S7 300/400 driver. You find more information in the following Link: http://support.automation.siemens.com/WW/view/en/24256006 (3) That is not possible! Bye |
Follow us on