(0)| 1/14/2022 2:13 PM | |
|
Joined: 10/15/2007 Last visit: 6/4/2024 Posts: 46 Rating:
|
Hi Thedrunkfish, because you mentioned "device failure" I would assume you mean "Device error" (some kind of firmware exception which requires contacting Siemens as user cannot fix issue itself). This would be indicated by all three LEDs - RN (RUN), ER (ERROR), MT (MAINT) - flashing at the same time. If so I would suggest to check if you are using latest 3RW5 firmware versions: And also recommend contacting Siemens support directly: Equipment Manual - SIRIUS 3RW55 and 3RW55 Failsafe Soft Starters In case you are not speaking of an "Device error" like mentioned above it might be helpful if you could provide information about which diagnostic error exactly is shown and needs to be reset. kind regards |
Last edited by: LostMyMind at: 01/14/2022 14:14:27Last edited by: LostMyMind at: 01/14/2022 14:35:52Last edited by: LostMyMind at: 01/14/2022 16:53:43 |
|
Follow us on