(0)| 1/13/2022 11:41 AM | |
|
Posts: 2 Rating:
|
Hello, I have an issue when I am trying to release the faceplate with the script. I made a simple faceplate with the text box. I would like to update a text field with the script. When I am trying to release the faceplate I receive an error (In attachment). I also tried an empty script and the result is the same. In the inspector window, I don't receive any information about the error. But when I select dynamization of the text field "None" I can release the faceplate without an error. Do you have any suggestions on how to solve the issue? Cheers, Aljaz ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/14/2022 08:42:10New subject after splitting |
|
Follow us on