(2)| 1/19/2022 1:14 PM | |
|
Joined: 12/18/2014 Last visit: 1/17/2026 Posts: 36470 Rating:
|
You can download the free upgrade to the current LSC version V8.3 from here: Download for LOGO! 8.3 Software UpgradeBut note: The download is subject to an export restriction, which requires advanced registration. Why do you have to log in and register for downloading export-restricted software and what data do you need for this?The upgrade can only be installed if a full version is installed on the hard disk or a full version is available on an installation medium: How do you install a downloaded upgrade for LOGO!Soft Comfort with or without installed LOGO! software?If you have (or buy) a new LOGO! (currently the current LOGO! is a LOGO! 8.3), then you definitely need LSC V8.3. With V8.3 you can create programs for all LOGO! devices (even older ones) or edit old programs and also load programs into older LOGO!s or load them from older LOGO!s onto the PC. |
This contribution was helpful to
|
|
| 1/20/2022 8:32 AM | |
|
Posts: 3 Rating:
|
Thank you very much for your assistance. |
This contribution was helpful to
|
|
Follow us on