(1)| 1/24/2022 7:01 AM | |
|
Joined: 5/3/2017 Last visit: 12/5/2025 Posts: 673 Rating:
|
Hi ashadako,
If you want to use simple logic if you use only SFC and CMTs you can use functions of CMTs. Functions are CMTs that has only one level in the technological I/Os. And you can integrate in a CMTs do add the functionality of function to the CMs. For more details to the function in the context of CMT see the application example Control Module (CM) Technology - Efficient Engineering with SIMATIC PCS 7. In the chapter 2.10 you can find the general description of the function and in the chapter how to create and integrate a function in to a CMT. With regards |
This contribution was helpful to
|
|
| 1/24/2022 9:30 AM | |
|
Joined: 8/1/2019 Last visit: 12/8/2025 Posts: 304 Rating:
|
its so unflexible to work with CMTs and SFCs |
Follow us on