(0)| 12/11/2021 4:19 AM | |
|
Posts: 8092 Rating:
|
Hello Kulet, 300608 - Speed controller at its limit, i.e. motor is blcoked means set torque limit is exceeded. Is Y axis is verticle axis? If yes, please check its counter balance cyclider pressure, bearings in sprobket, chain, external etc. etc. Also check if motor is brake motor. If yes, check motor brake release function. Hope this helps. |
| 12/15/2021 2:27 AM | |
|
Posts: 11 Rating:
|
Thanks for replying PISCEAN. The Y axis is on the horizontal table of the mill, it's a 3 axis machine Z is the vertical. The Y axis doesn't have a brake feature on the Z axis. I'll remove the way cover and see if there's any blockage or causing it to create this error.
|
Follow us on