(2)| 2/22/2016 7:12 AM | |
|
Joined: 3/14/2008 Last visit: 1/15/2026 Posts: 2233 Rating:
|
Hello Stephen, I've got the explanations for you: @100%s@ = Computername @101%s@ = Application name @102%s@ = User name @103%s@ = Comment (in long term archiving. A comment must be entered to display this Furthermore, you can also use the following placeholders for example: single messages, using the following data types: Byte (Y), Word (W), DWORD (X), Integer (I), DoubleInteger (D), Bool (B), CHAR (C) and REAL (R) eq: @1Y%d@, @2W%d@, @3W%d@, @3X%d@, @5W%d@, @6Y%d@. For example: "@2W%d@ references the second associated value as "WORD". |
Last edited by: Oreca at: 2/22/2016 7:24:53 AMIf I could help you, you can use the RATE button. Thank you. |
|
Follow us on