(0)| 4/1/2009 10:25 PM | |
|
Posts: 1690 Rating:
|
Hi, to solve your problem should be possible - but it needs a little bit more programming: a) You must define additionaly a time (=time window) in witch the pulses should be count periodic and then you can get the counter value and calculate the two numbers of pulses for the two outputs. Perhaps you can modify and use my circuit at "Display of scaled High Speed Input Values", Attachment: it counts the pulses over a time window defind into the pulssgenerator and let use the result of measuring of the window time before. That means you calculate and send pulses to the outputs and in this time the counter counts the next basic value.... b) you must send the calculated number of pulses: use a puls generator to control two counters ans set the ON and OFF parameters over a pointe with the calculated puls numbers to stop over a marker block the puls generators if sent the pulses to the both outputs Best regards Betel |
Follow us on