(0)| 3/29/2022 6:06 AM | |
|
Joined: 1/11/2019 Last visit: 11/24/2025 Posts: 899 Rating:
|
Hello Som@1994, Whenever we open a lower version of PCS7 project with higher version of PCS7, We have to do one of the function from below two points.
And then compile and down load the project. Kindly go through the below thread to work on above two functions. Manual for Migration to PCS7 V9.0 Note: Kindly have a separate backup of PCS7 V8.2 project |
Follow us on