(0)| 4/10/2022 9:57 AM | |
|
Joined: 9/17/2019 Last visit: 2/25/2025 Posts: 3 Rating:
|
Hi I have Process Historian 2014 and IS installed in a server which need to get datas from WinCC professional V16 which is installed from another PC. Configuration done as the SIEMENS manual "106264271_Installation_IS_PH_en" but unable get connected each other. 1) Both PCs have same user name and in "workgroup" 2) PH Ready component is running in WinCC PC. 3) All services mention in the given manual enabled and running. 4) No data source is showing in the PH console. 5) Connected clients in the console shows "0" in the PH console. 6) Status of the PH in the console "Idle", "start" given from the console with bring the Status back to "Idle". Please suggest if anything else need to to taken care to run the PH with data collection. Attaching the documents and screeshots Regards Anand R ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 04/11/2022 14:48:36New subject after splitting |
|
| 4/11/2022 2:50 PM | |
|
Joined: 8/21/2014 Last visit: 12/19/2025 Posts: 1098 Rating:
|
Closed, cause question posted twice. The second thread with the subject [Process Historian is not connecting to WinCC database ] is published within the conference [Process Control Systems SIMATIC PCS 7]. Best regards HH |
|
My Forum is the place to personalize your profile, |
|
Follow us on