(0)| 10/4/2021 3:09 PM | |
|
Joined: 10/17/2007 Last visit: 1/18/2026 Posts: 4579 Rating:
|
I attached 840D alarm list, from your statement --you have a running machine. if no one made any HW or SW ,parameter change. you need check your C44 axis control card and power section (someone call it drive). you can easily find the faulty drive --it will have red led on the front of control card. I suggest 1st step check encoder cable and motor cable connecting, then check control card number , if you have same card in the machine of another axis, sweep to try. that will be simple, after change card you will know . next step is check or replace power section (drive, possible 15A or 25A and so on) , the last step is check motor itself please feedback
AttachmentDA_1102_en.pdf (548 Downloads) |
Last edited by: nulizhang at: 10/04/2021 15:10:51If you like my comments please |
|
Follow us on