(1)| 4/21/2022 8:12 AM | |
|
Joined: 3/14/2008 Last visit: 1/15/2026 Posts: 2233 Rating:
|
Hi, Unfortunately this will mean you have to adjust faceplates and the scripting behind it in order to create such a functionality (which I do not recommend). Maybe another way is to write the tag value 2 or 3 based on the user authorization level, like when you login to WinCC, this will require knowledge of C-script/VB script. |
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
|
|
Follow us on