(0)| 12/15/2008 8:54 AM | |
|
Joined: 3/21/2006 Last visit: 1/10/2026 Posts: 10247 Rating:
|
Hello In MM440 part: Using binectors/connectors a flexible interconnection of process data can be created. The parameters r2050 and P2051 are used to display the data received by the inverter and select the data to be sent from the inverter. r2050 displays the setpoints and control words received by the PROFIBUS optional board. The parameter P2051 is used to select the signals (process data PZD), In receiving site CCR (central control room) it's depend what hardware you'll use to control the process. If you use Simatic S7 CPU use SFC14 to read this data from Drive via Profibus. About Simatic S7 this example is usefull: http://support.automation.siemens.com/WW/view/en/22813212 regards |
Last edited by: UMENCHO at: 12/15/2008 9:26 AM |
|
| 4/7/2009 8:34 PM | |
|
Posts: 2 Rating:
|
dear rico see P r0039 for see KWH. |
Follow us on