(0)| 5/9/2022 3:17 PM | |
|
Posts: 101 Rating:
|
Hello all, My Project is at PCS7 V9.0 SP3. So I installed APL 9.1 and the basic library 9.1. at Options / Charts / Update block types and did the procedure we know -> I came across below error for project specific blocks. Error Log File for CFC/SFC ... 04/26/22 - 00:40:41,0xEE0503E5,0xFF010205,0xFF010205 0xEE0503E5 92 SRV_BLOCK_UPDATE =SYSTEM_ERROR Programming error. 0xEE0503FF 30 SRV_BLOCKTYPE_BLOCKS_UPDATE =SYSTEM_ERROR Error being passed on. 0xEE0503FF 581 SRV_S7_BLOCKTYPE_UPDATE =SYSTEM_ERROR Error being passed on. 0xEE0503FF 12 TYP_S7_BLOCKTYPE_UPDATE_V6_0 =SYSTEM_ERROR Error being passed on If any one come across these kind of errors, Please suggest solution. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/10/2022 09:19:31New subject after splitting |
|
| 5/10/2022 9:20 AM | |
|
Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject While migrating to v9.1 SP1, Block type update fail with below error. is published within the conference Process Control Systems SIMATIC PCS 7. Jen_Moderator |
Follow us on