5/19/2022 7:55 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello MaCorMa, Welcome to forum. You should have open this post in SINUMERIK CNC automation systems product conference since it is related with NC system. Now to your query, please set axis (of which you want to replace encoder) MD 34210 = 1, switch off power & after replacement of encoder, move axis to known position (i.e. at 0 position) in JOG mode, select JOG + REFERENCE mode & set/modify MD34210 from 1 to 2, the axis reference position will set to 0. Before doing so, I suggest you to check parameter setting of topology comparison set, if it is high, system may display alarm when you replace encoder. For more detail information about topology comparison parameter setting, please refer Replacement of S120 componenets topic. Hope this helps.
|
Follow us on