(0)| 5/25/2022 4:15 PM | |
|
Joined: 5/16/2016 Last visit: 9/24/2025 Posts: 42 Rating:
|
Hello, Have you tested the connection to the directory? You can do it by the following: 1.Open BCC (Batch Control Center) 2. In the Menu Bar, click Options > Settings > Project Settings 3. In the Project settings window, expand Batches and select Archiving 4. Under the technology options you should see the path under the Directory. Make sure you are using the UNC convention. 5. Click the Test button, you will get a message displaying the results of the test. If the test fails make sure you have the correct user settings. Most setups I have granted read/write to everyone group for the target directory. Also review section and compare your setup to 7 of Part F - Industrial Security https://support.industry.siemens.com/cs/ww/en/view/109782722 |
|
Why you troubleshoot? |
|
Follow us on