(0)| 6/1/2022 10:20 PM | |
|
Posts: 8 Rating:
|
Hello, Im trying to use a internal timer to active a transition, i put on "true" the _I0 of my timer, but the times never counts. Could someone help me please |
| 6/2/2022 9:24 AM | |
|
Joined: 3/14/2008 Last visit: 1/15/2026 Posts: 2233 Rating:
|
Hi, When you declare a timer in SFC characteristics, you can fill in a "Initial value" for the time. If you haven't done so, you need to set TIME0 parameter. This is the duration of the timer. |
|
If I could help you, you can use the RATE button. Thank you. |
|
| 6/2/2022 9:27 AM | |
|
Joined: 1/11/2019 Last visit: 11/24/2025 Posts: 899 Rating:
|
Hello MarianoB94, The timer will not start/count without any trigger bit. Kindly use some bits to trigger the Timer. You can go through the below link which some user have faced the same issue earlier in forum, It would help you to get the solution. SFC - time delay between steps as parameter I hope it helps you! |
Follow us on