6/15/2022 9:21 AM | |
Joined: 10/8/2018 Last visit: 6/5/2025 Posts: 4 Rating:
|
Dear Team , I am having Max rated Velocity is of 154mm/sec, i am changing the velocity setpoint accordingly and the velocity override is 100%. P2646=100% P2643=0.2 1000LU/min If i set the velocity Setpoint below 1 1000LU/min then also the output of position controller is set to 1 1000LU/min and my motor runs at 13 rpm. i am not able to get speed below 1mm/min( 1 1000LU/min). Also if i set velocity setpoint p4643=0 and override p4646=100% and if position setpoint change then my motor runs at the velocity of 1 1000LU/min= 1000LU/min. How can i get the velocity setpoint below 1mm/min. like 0.2*1000LU/min =200LU/min. In my case 1000LU=1mm. Please help me geting the velocity Setpoint below 1mm/min or 1000LU/min so that i can deliever max accuracy. ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 06/16/2022 19:59:46New subject after splitting |
|
Follow us on