(0)| 4/17/2009 6:04 PM | |
|
Posts: 54 Rating:
|
Hi samkcr Yes, TM module will definitely help you in this. The TIM module supports both IEC 870-5-101 and IEC 870-5-104 protocols. The new TIM provides an integrated Ethernet interface with the IEC 870-5-104 protocol. In addition to Ethernet interface it supports serial communication also. I think TIM falls under Siemens PTD division. Have a look of the attached doc. Regards, Kanag AttachmentVICOS-RTU_E.pdf (307 Downloads) |
Follow us on