(1)| 7/9/2022 10:17 AM | |
|
Joined: 9/9/2015 Last visit: 12/5/2025 Posts: 732 Rating:
|
Hi, If i were you, I will propose to upgrade all the stations to PCS 7 V9.0 SP3 UC04. From PCS 7 V9.0 SP1 to SP2 are "Hotfix" upgrade. V9.0 Licenses will be usable for PCS 7 V9.0 SP2 or PCS 7 V9.0 SP3 UC04. Just like windows patch , antivirus definition upgrade or your mobile phone Apps update, you should always keep your application up to date to avoids known bugs. Hope this is helpful. |
|
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to
|
|
| 7/10/2022 10:02 PM | |
|
Joined: 11/19/2018 Last visit: 12/29/2024 Posts: 35 Rating:
|
This way in not permitted by my boss, could you introduce another way? |
| 7/11/2022 1:01 PM | |
|
Joined: 10/26/2011 Last visit: 1/13/2026 Posts: 766 Rating:
|
Hi memoll2012, You will receive the IPC with installation DVDs. You have to uninstall the IPC, install only Windows via the provided Restore DVDs and then your existing PCS 7 version. |
|
SIMATIC PCS 7 - Overview |
|
This contribution was helpful to
|
|
| 7/12/2022 3:20 AM | |
|
Joined: 9/9/2015 Last visit: 12/5/2025 Posts: 732 Rating:
|
Hi, When you buy spare IPC with pre-installed PCS 7 V9.0 SP2, once you power on the brand new IPC, you have the option to choose to load "A1" image or "A2" image. A1 image is without PCS 7 Installed and A2 image is after PCS 7 V9.0 SP2 installed. just go ahead and load back A1 image and install PCS 7 V9.0 SP1 yourself. Hope this is helpful. |
|
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to
|
|
| 7/19/2022 2:37 PM | |
|
Joined: 9/9/2015 Last visit: 12/5/2025 Posts: 732 Rating:
|
Hi, So, you load the A1 image, and install PCS 7 V9.0 SP1. But, by default, the automation licenses manager is empty, you need to put license in order for you to use the system. Now, you dont transfer the license into this station, thats all ya. If you talk about the windows license, by default, this license is already built in in the hardware. After you get the system online, the windows will be activated automatically. I dont think you can extract out the windows licenses. Hope this is helpful for you. |
Last edited by: JazTai at: 07/19/2022 14:38:15Please give me 5 stars Rating if my post is helpful for you. :) |
|
| 7/19/2022 4:40 PM | |
|
Joined: 10/26/2011 Last visit: 1/13/2026 Posts: 766 Rating:
|
Hi memoll2012, If the licenses are already on the computer, please remember to restore the licenses before formatting. The licenses are only valid for the full version including all Service Packs and UpdateCollections. As an example, if you have purchased licenses for PCS 7 V9.0, these are also valid for PCS 7 V9.0 SP1, V9.0 SP2, V9.0 SP3, but not for PCS 7 V9.1 or V8.2.
|
|
SIMATIC PCS 7 - Overview |
|
Follow us on