7/17/2022 7:32 PM | |
Joined: 7/17/2022 Last visit: 7/17/2022 Posts: 1 Rating: (0) |
How does one solve this? |
7/19/2022 11:42 AM | |
Joined: 8/12/2021 Last visit: 9/24/2024 Posts: 324 Rating: (29) |
Hi Zambia_Automator! It seems that the PLCs are not accessible. Is the system configured correctly in the project? |
If this Information really helps, you could use the Rate function |
|
7/19/2022 8:06 PM | |
Joined: 7/5/2013 Last visit: 9/26/2024 Posts: 3114 Rating: (512)
|
Hi Zambia, you may have a look in the following FAQ: What should you watch out for when downloading WinCC Runtime Professional from the Engineering Station to the Operator Station (Runtime PC)? Regards, Frink |
Pi is exactly three! |
|
This contribution was helpful to1 thankful Users |
Follow us on