(0)| 7/30/2022 9:39 AM | |
|
Joined: 12/18/2014 Last visit: 1/18/2026 Posts: 36470 Rating:
|
Import of a technical question via PM from the 123Nilessimmons Siemens 840c 1995 model Hello, We bought the Niles n20 cnc lathe from australia. When we bring the machine to our factory, the machine gives an alarm. And we found the reason. The machine was previously working in the automation system. Therefore, the machine was not ready because we could not connect a robot to the machine. 2 dmps do not work in Dmps with input modules. One of them is a robot and the other is a PC input for machine tracking. Can we delete them from within the plc program? Or will the machine be garbage? H8A24=roboter H8A25=operating panel AttachmentPictures.zip (217 Downloads) |
Last edited by: ixo65 at: 07/30/2022 09:57:47 |
|
This contribution was helpful to
|
|
| 8/1/2022 9:41 AM | |
|
Posts: 6 Rating:
|
Hello Opel Wien GMBH GENERAL MOTORS |
Follow us on