(0)| 8/5/2022 9:03 AM | |
|
Joined: 5/3/2017 Last visit: 12/5/2025 Posts: 673 Rating:
|
Hi cristian021091, when you install a SIMATIC or TIA program on a PC the installation setup will install also the Automation License Manager (ALM). The ALM is used to manage license keys (the technical implementations of licenses). And the software products requiring license keys automatically report this requirement to the Automation License Manager. When the Automation License Manager finds a valid license key for this software, the software can be used.
So every transfer of the license keys and the licensing of the software is done via ALM. You only have to ensure that the ALM on the PC have access to the specific license key, that the software needs.
There are two options.
The best manual which software needs which license is the manual SIMATIC PCS 7 Standard Architectures, but it is not really good. But you don't have to worry, if you transferred the licenses key to the wrong PC the PC which needs the software will display that a licenses is missing and in ALM you can get the information which licenses is missing.
The upgrade of a licenses key is really easy.
With regards |
Last edited by: Heisenberg2 at: 08/05/2022 09:13:03 |
|
Follow us on