(0)| 8/3/2022 5:08 AM | |
|
Posts: 3 Rating:
|
hi! i commissionning a drive 6RA8031with the BOP when i send the power on via terminal 12 the run state r0002 show me 12 meanning 12: o1.2 Wait for operating enable (signal source acc. to p0852) i check the p0852 and all is set to 1 but same thing and the drive not start how to solve it, also i try to connect on the CUD with starter via pc adapter usb but it not working please help ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/03/2022 08:52:11New subject after splitting |
|
| 8/3/2022 5:49 AM | |
|
Posts: 8092 Rating:
|
Hello, Welcome to forum. Please open new topic instead posting your query in old topic. Please refer SINAMICS DCM, List Manual, Firmware version 1.5 (based on 5.1 SP1) manual function diagram no 2580, drive control word enable input is made ON by an AND gate, i.e. p0852 & r53010.4 must be ON. r53010.4 is made high when DI 2 i.e. X177:13 is ON. So please check & ensure that DI 2 - X177:13 is ON i.e. drive operation is enabled. Hope this helps. |
Last edited by: PISCEAN 2010 at: 08/03/2022 05:54:15DI number corrected Last edited by: Jen_Moderator at: 08/03/2022 08:53:33Link optimized. |
|
Follow us on