(0)| 6/22/2020 12:30 PM | |
|
Joined: 11/18/2016 Last visit: 1/8/2026 Posts: 3 Rating:
|
Hi all, We've an installation where we control a plant with a 1214 FC and a ET200SP.The installation is running for over a year without any issue. the last 6 months we are facing some issues. The ET200SP lost its connection at some random times. mostly during night (between 10 pm and 6 am ). sometimes is also happens during the day. The 2 main errors we've received are " User data failure of hardware component" and "IO device failure - Watchdog time expired". I've already increased the Watch dog timer, but it didn't help. The CPU and ET200SP device are in the same cabinet and are power from the same source/ fuse.In addition there is also a UPS. So I highly doubt it's a power issue. I've added the error log to this post. thank you very much in advance, AttachmentDiagnostics.txt (950 Downloads) |
This contribution was helpful to
|
|
Follow us on