(0)| 8/16/2022 8:25 AM | |
|
Joined: 7/9/2017 Last visit: 7/1/2025 Posts: 1 Rating:
|
I want to place the servo motor with an external encoder. At high speed, it retracts and flies away. The external transmitter is a bar code reading camera that communicates with the drive controller via an SMC 30 module via an SSI interface. I am using Starter for this project. I get the value of the position from the camera, but the control is not correct, the motor starts jerking at high rpm. If anyone has an idea of what parameters to set, I thank you in advance. I have attached the project. Attachmentsiemens_forum.zip (588 Downloads) |
Last edited by: ttiibbii at: 08/16/2022 08:27:00Last edited by: ttiibbii at: 08/16/2022 19:17:40 |
|
Follow us on